XMC Pinout Tool 
------------------------------------------------------------------------------
V2.1.14
	- NEW: Support for XMC1400 LQFP-48 added
------------------------------------------------------------------------------
V2.1.12
	- Fix: USIC_1 DOUT in P0 were not shown for XMC1400
------------------------------------------------------------------------------
V2.1.10 
	- FIX: Comments longer than 13 characters are not stored
	- FIX: XMC3200 device has been removed
	- NEW: For future extend: separator character in pin name (e.g. U0C0.DOUT)  
		   must be specified for each module separately
------------------------------------------------------------------------------
V2.1.8 
	- New: Support for XMC1400 TSSOP38 added
------------------------------------------------------------------------------
V2.1.6
	- FIX: EBU.RD_WR# could not be found
------------------------------------------------------------------------------
V2.1.4 
	- NEW: Support for XMC4300 added
------------------------------------------------------------------------------
V2.1.2 
	- FIX: XMC44/47/48: Missing input clock pins for the DSD (MCLKxC, MCLKxD)
	- CHANGE: XMC12/13/14: Naming of ACOMP peripheral changed 
			  to "Ana. Comparator"
	- CHANGE: XMC47/48: Pin position of RTC_XTAL1 swapped with RTC_XTAL2
------------------------------------------------------------------------------
V2.1.1 
	- FIX: XMC1400 does not show USIC1 modules for all peripherals 
	       using the USIC
	- FIX: XMC1400 CAN RXD pins are not visible
------------------------------------------------------------------------------
V2.1.0 Version with new features and support of new XMC devices 
	- HINT: JAVA Version 8 is required
	- NEW: Support for XMC4700, XMC4800, XMC1400 added
	- NEW: Colour code for pins belonging to the same module e.g. USIC0_CH0 
	- NEW: Migration to other devices and package supported
	- NEW: Pad type is displayed for each pin by symbols
	- NEW: Detailed reporting when older configuration files are loaded
	- NEW: Power supply pins are marked with colour in the table view
	- FIX: Tool can also be started from USB sticks and network drives
	- FIX: Several fixes and improvements of peripherals
	- HINT: Renaming of some peripherals and signals done(when loading old 
		pinout configuration files a report will be generated)
------------------------------------------------------------------------------
V2.0.0 Version supporting all devices and packages of the XMC1000/4000 
	- Hint: old pinout configuration files are not compatible and 
		cannot be loaded 
	- 2nd window with table view of all pins added
	- User comment can be added to each pin
	- Meaning of colours is consistent: 
		black=unused pin/module, 
		grey=allocated pin/module, 
		red= mutiple selection of pin/module
	- New peripheral "HR-PWM" added for XMC4400 and XM4200 
	- New peripheral "Watchdog" added for all devices
	- New peripheral "Generic EBU" implemented for XMC4500
	- New peripheral "Generic EBU" implemented for XMC4500
	- USB Peripheral: VBUS signal added for XMC4500 and XMC4400  
	- Renaming of some peripherals and signals
	- Renaming of some packages
------------------------------------------------------------------------------
V1.0.0 Initial version with support for XM4500, XMC4400, XMC4200
	Known Bugs: 
	- USB Peripheral: no VBUS signal for XMC4500 and XMC4400 
	- HR-PWM missing in XMC4400 and XM4200
------------------------------------------------------------------------------